Hii guys,
I’m having a simple question but important for my project. Working with the [MLX90640 110 degrees IR sensor. Using the example code 2 right now and I’m getting the temperature array through I2C. My question: what is the structure of the array?
First the X values of the first Y row? Than the X values of the next Y row?
Thanks in advance.](SparkFun IR Array Breakout - 110 Degree FOV, MLX90640 (Qwiic) - SEN-14843 - SparkFun Electronics)