Qwiic Flex Glove Controller

Hello,I used this sensor Qwiic Flex Glove Controller and want to ask some questions:

  1. Is there only one address on a sensor (Finger1 and Finger2 are the same address 0x48)? Is there a way to use two addresses on the same sensor for Finger1 (0x48) and Finger2 (0x49)?

  2. After the sensor is connected, I still need to transmit the sensor data through bluetooth. Will it affect the sensor if using bluetooth?

Thanks!

Refer to the emails I had sent you personally previously, please…this is extremely simple and covered by the links in the hookup guide that have already been sent.

Also please do not create multiple topics/threads for singular issues

OK,thanks.

Can Qwiic flex sensor be connected to bluetooth?