qwiic.list_devices() command displaying wrong device

If I run the qwiic.list_devices() command from my jetson nano 4GB JP441

running python 3.6.9 and I have the qwiic micro oled attached via the pHat v2 board,

the device comes up as [(61, ‘Qwiic 4m Distance Sensor (TOF)’, ‘QwiicVL53L1X’)].

Is this just an error in the listing, as the micro oled display works fine, and has I2C address of 61d or 0x3D which is the default address

Sounds like a bug in the Qwiic_Py library, if you can [file an issue here, the library author may be able to take a look.](Issues · sparkfun/Qwiic_Py · GitHub)