I was wondering if it’s possible to connect my Qwiic shield to a mega2560? A program I need to run requires too much space and when compiling, I get this message:
“data section exceeds available space in boardGlobal variables use 14286 bytes (697%) of dynamic memory, leaving -12238 bytes for local variables. Maximum is 2048 bytes. Not enough memory; see http://www.arduino.cc/en/Guide/Troubleshooting#size for tips on reducing your footprint. Error compiling for board Arduino Uno.”
I need to use a spectral sensor specifically designed with the i2c system.
Please advise.