Qwiic RFID wrong readings after 20 reads

:frowning: too bad since the reader we are discussing here is the only Qwiic RFID reader from Sparkfun.

Sparkfun offers the M7E Hecto, but that one is 10 times the price ($300) and has no Qwiic, so no option at least for me.

Then there is the Sparkfun USB-C Reader, price is OK, no Qwiic but pin breakouts, only problem is I do not know if it can be used without USB-C (hookup guide is not clear about that) and I cannot see how to connect that one to the Micromod Single mainboard as I already must use RX/TX for the BNO086 IMU RST/INT signals.

I could not find an Adafruit Stemma/Qwiic compatible alternative; Adafruit offers a Stemma/Qwiic compatible RFID tag, but no reader.

It would be great if Sparkfun replies to this topic as it clearly shows that the product is broken as it is sold/in stock with resellers at the moment.Are there are any solutions or plans about the issue @TS-Russell ? Anyone internally where you could forward that issue to?