Hi,
I have an urgent request on a problem I have been facing for 2 weeks. I read all the spec sheets carefully, looked at the Arduino examples and libraries and various trial and error with no luck.
My setup is as follows: I am using I2C from a zigbee and connect directly into the Qwiic Scale through hole connection (not using the qwiic connectors). I tie 3.3V from the xbee to the AVDD (same voltage i apply to 3V3 throught hole on the qwiic scale board). I reset all registers, did the NAU7802 Analog front calibration already. The readings are jumping around but I know it’s sort of working since when i put the load on it, the overall numbers do go up. When i say jumping around, i mean at zero for example, it would jump from 4000 to 12000, etc. So I don’t think those are noises. When I use the HX711, they are good (jumping within a relative range) with the raw numbers.
Is there something I am missing? I am guessing it must be…
Thanks!