Hello there,
i hope you are all well…
I have this question on the R4-5A RGBW Receiver…
-----------------------------------------------Spec-------------------------------
Working Frequency 2.4GHz
Working (Input) voltage DC5V~DC24V
Max current load 5A x4CH Max 20A
Max output power 240W (12V)
Remote Distance 30m
since its POWER output is 240W, does that mean it only transmit the data to only LED STRIPS of max 240W?
for example:
i am gonna use the following led strip.
Led strip rgb 5050 SMD 12v 60Led ip65 75w 5Meters
so, how many LED strips does the above receiver support?
if i am installing a 100Meters of the above led strips in FIXTURE, how many receivers of the above do i need?
Thank you so much