A novice needs help… new to electronics age … know absolutely nothing about programming. I need help with components and programs. I inadvertantly posted this in code snippets. ![]()
I am wanting to start a remote pump, 600 ft away, have it run for a preset period of time [adjustable time range from 30 to 60 minutes using a spring wound, non powered timer to initiate start and stop]. 3-5 cycles/day.
I would like to use a low powered radio system… initiate the start signal thru the timer, and send to a remote transciever, where a start signal would be applied to start a large pump thru an interposing relay. A pushbutton or selector switch will be in series with the initiating timer contact to allow stopping of the pump early, or in an emergency.
The terrain between the pump and the remote location is rough, so I will need to elevate the antenna at the pump transceiver to get good line of sight.
There is no power available at the transmitter, so I would like to use a 12vdc battery with a solar charger to supply power.
At the pump, I have 120vac, 1 phase available for control power, or feed to power supply for receiver.
Low installed cost and reliability are important. :roll:
Electricrandye