I’m new to electronics and would be grateful for any expert advice on the following situation
I’ve built a basic circuit to try show how a transistor works as a switch. Basically, I have an NPN transistor hooked up to an LED, 6v power supply and 10k potentiometer.
When the pot is turned up enough the LED glows brightly- until it is turned up to that point, it glows not very much.
My question is: does this circuit demonstrate the transistor acting as a switch, or no? If no, is there some way with minor changes I could modify it (e.g. using a fixed resistor instead of the pot)?
An LED almost always requires a series current limiting resistor. A 1000 Ohm resistor is usually fine. Post a circuit diagram of how you wired everything and state the transistor type.
Hint: google “transistor switch circuit” for many introductory pages.
There is a clear on-off effect when the pot is turned up to a certain point- not a range of brightness. I think that is the transistor working as a switch. Am I right?
Also, with the previous circuit: would the components be damaged? As I shared this circuit (wrongly) and need to make ppl aware
There is a clear on-off effect when the pot is turned up to a certain point- not a range of brightness. I think that is the transistor working as a switch. Am I right?
Correct. The transistor needs a certain voltage/current to be fully switched on. The point of a transistor is to switch a high voltage/current device from a low voltage/current device. An example would be trying to get an Arduino to turn on a motor or a high wattage LED. The Arduino cannot supply enough voltage or current and if you tried it, it would smoke the Arduino. So we use a transistor to carry the current and keep it away from the Arduino.
Also, with the previous circuit: would the components be damaged?
You already know the answer, so why ask it again? If you wanted to keep the wrong schematic away from others, why not delete it?
This circuit needs a resistor to protect the LED, right?
The capacitor is 1000uF and more than 9v. The first switch is held down to charge up the capacitor, and the second to flash the LED (using the stored charge)
You need to provide a current limiting resistor nearly always (I’m sure there are cases where it’s not required although I really can’t think of one). Plan on it and design it in!