I’ve re-winded a (RC plane) bldc motor (1800KV, 12 pole, 16 magnets) with 26AWG wire 13 turns on each stator.
Before re-winding the motor was ok.
Now it doesn’t spin. Initialization with esc (and PWM) done properly (the tones of settings are as it should be).
But when I try to actually run the motor, it just shakes with high frequency beeps for few seconds and stops (seems it’s getting signal from ESC & trying to spin but can’t for some reason).
I’m using MCU (Atmega32) PWM signal (duty cycle controlled by a Pot(VR).
info: ESC(20A, non-branded) and Lipo battery(2s, Mystery 2800mAh).
Can anyone please help me?
note: I’m not using any remote control
Before re-winding it was delta now I re-winded it as star configaration.