Hi
I’m looking for a recommendation on a slim relay or contractor to use as a load on Qwiic Quad solid state relay to have both a normally open and closed circuit.
thanks
Hi
I’m looking for a recommendation on a slim relay or contractor to use as a load on Qwiic Quad solid state relay to have both a normally open and closed circuit.
thanks
Don’t have any to recommend unfortunately but you will need a relay with an AC coil rated for a minimum of 24 volts. An electrical supply warehouse should have something that would work for you.
Thanks.
Are these relays only intended to be used at 60Hz?
Would I need to find a 50Hz relay if I’m using 240v 50Hz?
I’ve also noticed that these relays retain memory and often need their I2C cable disconnected to erase. Is this something you guys have come across?
The relays will work with either 50 or 60Hz.
There’s no ‘memory’ in the relays, when you command one to turn on you need to send a second command to turn them off.