Actually what i planning i will use one programmer for flash download.
If i do this then is there any problem.
For this type of thing is it need to write code for boot loader.
The boot loader is built into the chips, and the manufacturers provide download programs to put a hex file into their chip via the bootloader.
I have one confusion on boot loader. I think It is use for Download the
program from PC to flash memory of controller. Is it Correct?
IF it is correct than is there any other application where we can use Boot loader.
You are correct.
I do not know of other uses of the bootloader.