Relay footprint from SparkFun Eagle library?

Hi everyone,

I want to design a circuit which controls 12VDC at max 30A, but I don’t want to route the 30A through copper traces on my PCB. So, I figured the Quick-Connect version of the relay that Sparkfun sells (COM-00101) will do the job fine. I’m kinda new to using Eagle, and I was wondering:

Is the device “RELAYPTH2” in the SparkFun.lbr library with package footprint “RELAY-T9A” the device I want to be using if I want to use the quick-connect version of the Tyco T9A power relay? :?:

Thanks!

I don’t seem to have a device named RELAYPTH2 in my Sparkfun library. I see the package footprint of RELAY-T9A in there though.

COM-00101 doesn’t appear to be the Quick-Connect version of the relay. The footprint for that would just have one hole on either side for the flange.

J