Hi,
I am completely non tech so please bare with me. I have recently completed a project for a local environmental group, which involves remote monitoring of live capture traps for feral pest animals. The system uses a small SMS unit which sends a text message to a supervisor when a trap is sprung. The power requirements are met by a solar panel and small storage battery. Cost is around $450(nz) for the complete unit. The sms unit is quite sophisticated, with two inward circuits and two outward.
It had occurred to me that if I could program an android smart phone there would be considerable potential savings, both in unit cost and in power requirements. I only require a single closing or opening a simple circuit to trigger either a pre worded text, or even just a pre set phone call. An android smartphone would have only a fraction of the power requirements of the existing SMS unit, with big savings in both solar panel and storage.
I came across the DEV-13613 ROHS and from what I can figure out might just do what I need. But I know my limitations and they are no where near what would be required. So was wondering if anyone would be interested in the above as a project which well have a potential commercial application in trap monitoring in New Zealand.
With thanks… Peter