My home (built in 1945), has an old “gravity” heater, which is basically a gas furnace under one central vent located in the middle of house under the floor. There is no forced air distribution at all, the hot air simply rises up the vent, and pretty much all of it goes up stairs and not into other rooms downstairs. That’s actually fine because we only need the heater in the middle of the night for a few hours, and all our bedrooms are upstairs. However, the thermostat is located downstairs and is too far from the vent in order to operate as an effective switch (it’s in the dining room which pretty much stays chilly even if even if it’s blazing hot upstairs.)
I would like to turn the heater on or off based on the ambient temperature upstairs.
I removed the thermostat cover and it is just a metal coil that expands and contracts, with a little magnet at the end that snaps onto another piece of metal to close the millivolt circuit. That explains why the thermostat is not very precise at switching on or off, the magnet holds onto the connection longer than it needs to.
The way I see it, there are 2 problems that need to be solved:
-
I need to be able to remote control the opening or closing of the millivolt circuit. a) I can do this manually by attaching an arduino + servo arm to move the existing thermostat temperature lever. or b) bypass the thermostat entirely using some kind of relay? But I don’t know enough about relays … what kind, how would it be wired up?
-
I need to be able to forward the ambient temperature upstairs to the arduino controlling thermostat downstairs. How do I do that? Is there a wireless temperature sensing product I can purchase and hack? Or do I just get another arduino upstairs, get ambient temperature using a thermistor, then wirelessly forward the measurement to the other arduino using a pair of xbees? I have never used xbees before. Should I consider wifi internet shields instead? That way I can potentially also control the heater with my phone/browser?
Thanks for any advice.