I now have 6 of the RF Link 4800bps Receiver. I have 3 at each range, 315Mhz and 434Mhz. I can not get any of them to work. I also have a old RF Link 2400bps Receiver that works fine.
I can put in the 2400bps receiver and everything works. I put in the 4800bpd receiver(All 6) and I get nothing. Not even static. Any one else having the same issue?
Am I being dumb with the code?
The 2400 and the 4800 are pin for pin compatible, aren’t they?
Did I blow them our in the 4in from the static bag to the bread board?
Here is my setup/code.
I have two Arduino’s. One playing TX and one playing RX.
The RX code
int incomingByte = 0; // for incoming serial data
void setup() {
Serial.begin(4800); // opens serial port, sets data rate to 4800 bps
}
void loop() {
// send data only when you receive data:
if (Serial.available() > 0) {
// read the incoming byte:
incomingByte = Serial.read();
// say what you got:
Serial.print("I received: ");
Serial.println(incomingByte, BYTE);
}
}
The TX code
void setup() // run once, when the sketch starts
{
Serial.begin(4800); // set up Serial library at 9600 bps
}
void loop() // run over and over again
{
Serial.println("Hello world!"); // prints hello with ending line break
delay(50); //spam the AIR!
}