RF Transciever project

Hello friends,

I have undertaken an RF based remote robotic axis control project.The theme is to use a keypad having 6 keys to be encoded and transmitted using RF module and then I need to recieve it into the robot and it will decode and control appropriate relay for necessary PLC operation.Now there’s been a mess with the type of RF module to use an how to pick up the data format for that. I have decided to use Maxim 1472(Tx) and 73(Rx). These are very easy to understand,yet I don’t have any practical realizable circuit to design…I tried it in MAXIM and googled,but it returned nothing expect despair.Can anybody suggest me a solution?..Is this SOC fine for my project or can I get a simpler Chip for this project?..And if yes, then could you tell me where to find such application circuit?..I need help soon.Thanks in advance…