RFM69HCW and Arduino Uno R3 Problem

I am following this tutorial:

RFM69HCW Hookup Guide

https://learn.sparkfun.com/tutorials/rf … okup-guide

For one node, I am using the RFM69HCW and a Arduino Uno R3.

This combination is not working properly for me.

I have it wired the same as for the 5V Redboard in the tutorial.

I am using the same code as in the tutorial.

When I start the serial window for it the line “Node 1 Ready” appears.

Then I do a send and the line “Sendin” appears and nothing else.

Then it either seems to hang up or the line “Node 1 Ready” reappears.

It’s reappearance tells me that the Arduino Uno has reset itself as this line

should only appear on startup.

Please comment.

I this exact set-up all the time and works perfectly so you must be doing something wrong or something is fried…

Did you use signal translators ? The Uno is 5V and the RFM69 is 3V.

AgroMe:
I this exact set-up all the time and works perfectly so you must be doing something wrong or something is fried…

Did you use signal translators ? The Uno is 5V and the RFM69 is 3V.

Thanks. At least you confirmed to me that this setup will work.

I did use signal translators but I noticed that the brown colored line (D2) in the tutorial has no translator.

Is this OK?

jack0987:
… I noticed that the brown colored line (D2) in the tutorial has no translator.

Is this OK?

Did anyone pick up on this?

Should the brown line (wire) in the tutorial have a 5V to 3V converter?

AgroMe:
I this exact set-up all the time and works perfectly so you must be doing something wrong or something is fried…

Did you use signal translators ? The Uno is 5V and the RFM69 is 3V.

Got it working now. A failed solder connection may have been the problem. I resoldered all of the connections

and checked all of the wires.

jack0987:

jack0987:
… I noticed that the brown colored line (D2) in the tutorial has no translator.

Is this OK?

Did anyone pick up on this?

Should the brown line (wire) in the tutorial have a 5V to 3V converter?

Did anyone pick up on this?

O is an output on the module and can safely be connected directly to an input on a 5V Arduino (e.g. the “brown wire”).

Usually, a 3V signal is recognized as a HIGH by a 5V Arduino, but for totally reliable connections, it is better use a logic level converter.