I’m making my first attempt to setup and RTK base station using a Sparkfun board. I have my GPS antenna mounted in a fixed location with a good view of the sky and have recorded about 6 hours of data using U-Center. I’ve then used RTKCONV to create and OBS file and submit it to CRCS for processing. CRCS responds nearly immediately with the following…Error : The RINEX file contains formatting errors in the observations at epoch 2024 4 9 11 53 7.00. Please correct and resubmit.
I’ll try to attach my OBS file for review
partialOBSfile.txt (3.15 KB)