I am looking for the mechanical dwg which shows all dimensions. I have ordered the board, however I need to start on the mechanical layout of my project. I especially need distance between 2 mounting holes and board size. Have looked everywhere. Thanks in advance.
There’s a 3D icon with the product image thumbnails. It didn’t work with my browser but it may work for you. There are also some other drawing files (Sketchup, STL, Blender) immediately below that that might have some dims.
I imported the board to KiCad. From the bottom edge (the one with the 6-pin straight header), the mounting hole centers are at 2.8 and 17.4mm up. Board size is 15.24 x 20.32 mm