Hi,
I am new with this board I have few questions:
- I can connect to this board via WIFI and get when I set gpio this is ok now the question is:
How to do this while I am connected to Home Router? - I lost the connection with WIFLY, I have tried to do the following:
scan 10
set wlan ssid
set wlan auth 3 (WPA2PSK)
set wlan phrase my password
set wlan join 1
set ip protocol 2
reboot
Now I try to connect via my but I can’t
Also the commands are ADHOC, and the configuration is TCPIP - can this work??
I can see that my router DHCP - is giving me new line - but I can’t connect to is and get the back
- Can I update firmware - after I downloaded new firmware to my LAPTOP?
What is the difference between same firmware versions (EZX-AP, GSX-AP)
- can this module send out WEB-PAGE when I connect it from outside? what do I need to do to work this out??
Thanks any answer will be appreciate!
Roee