Hi,
my question is not about a product bought from sparkfun. But I as I fail to get help from the manufacturers forum, I hope to find some help here.
It is about using PLL + encoder on the Romeo all in one board.
http://www.dfrobot.com/wiki/index.php?t … U:DFR0004)
As far as I understood it:
http://www.scribd.com/doc/52414546/12/P … LL-Control
the encoder should directly be hooked up to the PLL control.
With PWM I need to do the control via the code. But with PLL the electronics should do it by using the encoder as speed feedback signal.
How do I set this up?
Thanks
Robert