I have an MSP FET debugger (parallel). I have selected the /dev/lp0 parallel port. When I try to connect I get a “Device or Resource Busy” error.
Any Linux experts out there? How do I connect to the parallel port under Linux?
Thanks
I have an MSP FET debugger (parallel). I have selected the /dev/lp0 parallel port. When I try to connect I get a “Device or Resource Busy” error.
Any Linux experts out there? How do I connect to the parallel port under Linux?
Thanks
The obvious question: did you try to run it as the root user? (if it works as root, it’s probably a permission problem).
Update:
I have done the folowing:
mknod /dev/parport0 c 99 0 -m 666
and
chmod 777 /dev/parport0
now when I try to connect I get a “parallel port already in use” error.
Thanks
I tried running crossstudio as root, same result. ![]()
I checked the “allow port sharing” box in crossworks and it works.
Thanks