PaulZC
January 16, 2025, 7:35am
4
Hi Gregg (@wstefanc ),
I just wanted to make you aware that a couple of users have run into RAM issues on the Reference Station recently. I’m not sure if the 0000 issue is RAM related, but it’s a possibility. Links attached below.
I hope this helps,
Paul
I have configured my SparkFun RTK Reference Station to firmware version 4 and set up the SSID and password via serial. The reference station is connected to my network, and the IP address is displayed. However, when I try to connect to the IP address using Putty on my PC, the connection is being rejected. Could you please let me know if any additional configuration is needed to view the NMEA or RTCM messages in my Putty terminal via Wifi?
Hello everyone,
I am currently commissioning our second RTK Reference Station but have encountered a troubling issue: whenever I enter Survey mode, the station reboots continuously and never completes the process. Originally, the station shipped with firmware 3.5, and I tried upgrading it via the Wi-Fi config page, but it would reboot as soon as I clicked “Install.” As a workaround, I updated the u-blox ZED-F9P module firmware to L1/L2 HPG 1.51 using u-center over USB and then upgraded the Reference Station firmware to 4.1 with RTKUploader over USB. Following these upgrades, the firmware versions displayed correctly on the Ethernet config’s web interface, but after leaving the station off overnight, the Ethernet config page no longer shows the u-blox firmware. Additionally, the Wi-Fi config page still fails to work.
Now, whenever I try to cast to RTK2go and switch to Survey mode, the station reboots continuously, never staying on long enough to complete the survey or establish a data…