I have a RTK Reference Station that I installed in remote location I don’t have physical access to right now. It is connected to ethernet though.
I would like to
-
Configure it from an external network
-
Be able to download the .ubx file from an external network
If it is not a built-in feature of the Reference station to be able to configure from an external network, I can setup a pi with a vpn and connect to the Reference station over serial, but I would still need to be able to download the .ubx file to the pi over serial.