I cannot get to work more than one MMA8452Q accelerometer (I actually actually need 6 to 8) using a qwiic mux shield on a Arduino ONE.
I only get one to work when using the example provided by the documentation. This is only when connected to the standard arduino pins (not working connected to the shield pins)
I cannot understand however how do I manage to get information from different accelerometers at the same time. Is there any documentation or example I can have a look at? I can see that this might be a start point but I dont understand very well (I am an artist and I am better at programming that electronics and hardware sorry…)