Hi Magnus!
First to your questions.
SAMBA System recovery still not working! Not new Hardware will be recognized after i did:
Power off
set jumper Test
Power on
wait >10sec
power off
unset jumper Test
Power on
and the directly connect to the PC!
Is ist possible that there is no Boatloader anymore in the ROM or whereever!
If this is possible how do i get a new Boatloader on my Board?
The message “No valid processor ID found” came from SAM-BA!
The other message with…JTAG chain…occur from ecplise when i start the openocd routine!
Here is the message in detail:
make -k program
Flash Programming with OpenOCD…
'C:/Programme/openocd-2007re141/bin/'openocd-ftd2xx.exe -f 'C:/Programme/openocd-2007re141/bin/'at91sam7s256-armusbocd-flash-program.cfg # program the onchip FLASH here
Info: openocd.c:86 main(): Open On-Chip Debugger (2007-04-16 19:30 CEST)
Error: jtag.c:1230 jtag_examine_chain(): number of discovered devices in JTAG chain (578) doesn’t match configuration (1)
make: *** [program] Error -1
Now to your tip.
I changed the speed from 2 to 10, 20 or 30! Nothing changed! 
When i unplug the JTAG cable from the EK-Board i get another message in ecplise. The message says the the cable is not connected with the EK-Board.
That says me that there must be a way to fix it, but which way???
Do you have another idea?
For example how i get a new bootloader in this board? Perhaps with ecplise?
Thanks so far!
Best regards from Cologne
Tobi