I flashed the uf2 bin bootloader using the Jlink edu and studio 7 says flash was successful. But when i plug in the usb to board. I dont see it on the device manager nor the Arduino IDE. i made a custom board using the Sparkfun Micromod SAMD51 M.2 board. SparkFun MicroMod SAMD51 Processor
I complied the code on the Arduino IDE and then exported the compiled binary.
The following are my fuse settings
AC_BIAS0 = 0x01
ADC0_BIASCOMP = 0x07
ADC0_BIASREFBUF = 0x04
ADC0_BIASR2R = 0x07
ADC1_BIASCOMP = 0x07
ADC1_BIASREFBUF = 0x04
ADC1_BIASR2R = 0x07
USB_TRANSN = 0x09
USB_TRANSP = 0x19
USB_TRIM = 0x06
ROOM_TEMP_VAL_INT = 0x1E
ROOM_TEMP_VAL_DEC = 0x01
HOT_TEMP_VAL_INT = 0x69
HOT_TEMP_VAL_DEC = 0x00
ROOM_INT1V_VAL = 0xFE
HOT_INT1V_VAL = 0x01
ROOM_ADC_VAL_PTAT = 0xABA
HOT_ADC_VAL_PTAT = 0xD37
ROOM_ADC_VAL_CTAT = 0xB88
HOT_ADC_VAL_CTAT = 0x95C
BOD33_DIS = 
BOD33USERLEVEL = 0x1C
BOD33_ACTION = RESET
BOD33_HYST = 0x02
NVMCTRL_BOOTPROT = 0
NVMCTRL_SEESBLK = 0x00
NVMCTRL_SEEPSZ = 0x00
RAMECC_ECCDIS = 
WDT_ENABLE = 
WDT_ALWAYSON = 
WDT_PER = CYC16384
WDT_WINDOW = CYC16384
WDT_EWOFFSET = CYC16384
WDT_WEN = 
NVMCTRL_REGION_LOCKS = 0xFFFFFFFF
SW0_WORD_0 = 0x1E7079D (valid)
SW0_WORD_1 = 0x1B29 (valid)
TEMP_LOG_WORD_0 = 0xFE06911E (valid)
TEMP_LOG_WORD_1 = 0xD37ABA01 (valid)
TEMP_LOG_WORD_2 = 0xFF95CB88 (valid)
USER_WORD_0 = 0xFE9A9239 (valid)
USER_WORD_1 = 0xAEECFF80 (valid)
USER_WORD_2 = 0xFFFFFFFF (valid)