I’m trying to connect the teensy 4.1 board to the Sara r510aws evaluation board so I can send some data from the teensy 4.1 board to the Sara r5 board. What pin out connections would I need to make on the Sara r5 board to the teensy 4.1 board? I think I have to connect the TXD and RXD of the Sara r5 to the teensy board, but those pins are not available on the evaluation board. How would I proceed?
You could go about this a few different ways; take a look here https://www.pjrc.com/teensy/pinout.html for the teensy pinout
The easiest way would probably be to just declare DO and DI pins on the R5 in your sketch as being I/O, then wire them to your teensy’s pins…this example https://github.com/sparkfun/MicroMod_As … le6_IOPins might help
You could also use the i2c/qwiic instead…only caveat is that you’d only need to hook up SDA and SCL (not power/GND), so you don’t have the 2 boards’ voltage regulators arguing
You can scroll ~2/3 the way down here https://learn.sparkfun.com/tutorials/mi … e-overview for a chart of the pin #s/functions
Ok, thank you for your reply. So just to clarify, I can send the data over via I2C only by connecting the SDA and SCO pins from the R5 to the Teensy right? No other connections?
You need ground as well.
/mike
Ok thank you. I will try that and see if it works.
If I use I2C, wouldn’t i need the address of the sara r510aws board? How would i get that? Let’s say instead of the teensy, i use the arduino uno. pins 0 and 1 are rx and tx on aruino uno. how would i connect those to the pins D0 and D1 on the sara r5 board, and how would i declare them in the sketch so i can send AT commands from the sketch that i upload to the ardunio uno?
What are the UART pins on the SARA R510AWS Eval Board? I am not sure what the TX and the RX pins are on the SARA R510AWS board, please advise as soon as you can! thanks!
Looking at the schematic (https://cdn.sparkfun.com/assets/4/0/d/5 … ematic.pdf), it looks like the UART goes from the module, through IC1 and IC2 to convert them to 3.3v levels, and show up on the micromod connector on pins 13,15,17,19, 20, 22
Yeah I took a look at that. I figured it out now, and gotten it to interface with the teensy board. Thanks again for your help!