I'd have to run some numbers but I would think that distance do-able. I'll see if I can re-find that paper I saw on underwater absorption and scattering.turtle dude:
i would only be looking a range of 180-200m if possible?
There's 2 questions here, the location of the transmitter relative to the coverage area and the best location for the receive hydrophones;turtle dude:
The receivers would be mounted on the out side of the rebreather case (i might even mount them in seperate little housings with leads going back to the control unit to give more flexibility with location).the transmitter would be mounted approx 5-10m above the wreck attached to the shot line.
Re: the first … You can think of the beacon transmitter, using multiple “speakers” acting like a big search light, consisting of multiple flashlights. The diver needs to be in the area “lit up” by the search light. The transmitters you chose have a narrow “vertical” beamwidth, perhaps 15 deg (IIRC). I was surprised it wasn’t the same as the “horizontal” beamwidth but there you go. So the narrower the beam, the higher up from the sea floor the transmitter needs to be to “light up” all of the wreck and it’s immediate surroundings. See the diagram for the math.
In the above a single transmitter/speaker is aimed (blue line) just off vertically downward by 1/2 of it’s ([half power full) beamwidth. The beamwidth is indicated by the red lines. It will cover out to a distance R from directly below the beacon. As you can also see the distance from the beacon to the furthest point out in the coverage area is > R and > H. This is the distance to be used in calculations of how far away can/must the beacon be heard, = sqrt(R^2 + H^2).
re: the second … will mounting the receive hydrophones on the rebreather block them from getting a signal when the diver is swimming towards the beacon ? Does the aiming of the hydrophones change if the diver if floating vertically vs horizontally ? I have to believe this is the case but I’m unsure how much it’ll matter.
turtle dude:
so would it be a case of fitting more transmitters (ie six instead of four) to get the 360° required cover? Also if i had more transmitters if there beams crossed would this start to cause issues?
You should be able to add more and get the coverage needed. I am assuming that each transmitter is just a speaker and needs an amplifier to drive it. That way you can add any “tweaking” needed to get all the transmitters in phase with circuitry btw a common 40 kHz oscillator and the individual amps for each transmitter/speaker. How many more transmitters/speakers are needed is another exercise in geometry. I might need a beer or 2 to make a good diagram of that, one that’s accurate. It’s been a while since I did conic sections. :mrgreen:
http://en.wikipedia.org/wiki/Conic_section](Beam diameter - Wikipedia)