Im working on a device for a dance project that uses body-mounted IMUs to feed information to a processing sketch over bluetooth serial.
-There are three 3.3v Pro Minis (https://www.sparkfun.com/products/11114), each communicating with two IMUs over IC2.
-These feed data over Serial into a 3.3v Mega (https://www.sparkfun.com/products/10744). Each one goes into its own serial port on the Mega (Serial1, Serial2, Serial3).
-The Mega gets data from each Mini every time through loop(), and then when Processing asks for it, sends data in nine-byte chunks to a Processing sketch through Serial via a bluetooth module (https://www.sparkfun.com/products/12580).
-The Processing sketch reads the incoming data and moves stuff around on screen corresponding to input coming from the sensors.
-The Mega also monitors battery voltage levels over I2C using a Lipo Fuel Gauge (https://www.sparkfun.com/products/10617)
Everything above works perfectly. No problems anywhere. Problems begin below:
I want to have an SD card logging the sensor data on-board in case the Bluetooth connection craps-out during a recording (and as a backup), and I want to use an RTC to give the data context in time. I want to prompt the data-logging to start and stop from Processing.
I have tested the RTC (https://www.sparkfun.com/products/10160) and the SD card (http://www.adafruit.com/products/254). Both use SPI. Both work great with the Mega by themselves, and I did a test of logging the RTC data to the SD card each time through loop(), and that worked great too.
The problem is when I bring it all together. Just introducing the RTC works fine. I can send the time and date to Processing along with the IMU data. BUT: when I try to use the SD card, the info coming in to Processing FREAKS OUT! That is, I can move my IMUs around and see smooth changes on screen, and then when I enable logging to SD, everything starts moving randomly.
My code is below. Is there anything I’m missing? I have tried both the included SD.h library as well as the SdFat.h library. Below is the code for logging the actual data, but even if I change it to just write a constant variable to the SD card it still messes with the info going to processing.
Help?
#include <SD.h>
#include <SPI.h>
#include <Wire.h>
#include <RTClib.h>
#include <RTC_DS3234.h>
#include "MAX17043.h"
MAX17043 fuelGauge(20,10);
File myFile;
// Avoid spurious warnings                                     //This is from RTC Example code. Might not need it?
#undef PROGMEM
#define PROGMEM __attribute__(( section(".progmem.data") ))
#undef PSTR
#define PSTR(s) (__extension__({static prog_char __c[] PROGMEM = (s); &__c[0];}))
// Create an RTC instance, using the chip select pin it's connected to
RTC_DS3234 RTC(53);
char armR[8] = {0,0,0,0,0,0,0,0};
char armL[8] = {0,0,0,0,0,0,0,0};
char legs[8] = {0,0,0,0,0,0,0,0};
int led = 13;
int battStatus = 1;
boolean logging = false;
void setup() {
  pinMode(led, OUTPUT);   //LED setting
  pinMode(A7, OUTPUT);    //Mini 1 RST
  pinMode(A6, OUTPUT);    //Mini 2 RST
  pinMode(A5, OUTPUT);    //Mini 3 RST
  pinMode(10, INPUT);     //Fuel Gauge
  pinMode(A8, OUTPUT);    //SD Card
  
  digitalWrite(A7, HIGH);
  digitalWrite(A6, HIGH);
  digitalWrite(A5, HIGH);
  
  SPI.begin();
  RTC.begin();
  
  SPI.setDataMode(SPI_MODE0);
  
  
  // initialize all serial ports:
  Serial.begin(38400);
  Serial1.begin(38400);
  Serial2.begin(38400);
  Serial3.begin(38400);
  
  fuelGauge.begin();
  fuelGauge.setAlertThreshold(3);
  
  if (!SD.begin(A8)) {
    //Serial.println("initialization failed!");            //Indicate SD init error
    return;
  }
  
  
  
}
void loop() {
  
  const int len = 32;
  static char buf[len];
  DateTime now = RTC.now();
  SPI.setDataMode(SPI_MODE0);
  
  battStatus = digitalRead(10);
  //Serial.print(battStatus);
  if (battStatus==0) {
                                           //Battery Alert here 
  }
  
  
  
  Serial1.write(1);                        //Get data from ProMinis
  if (Serial1.available()) {
    
    int starter = (int)Serial1.read();
    
    if (starter==201) {
      Serial1.readBytes(armR, 8);
    }
    
  }
  
  Serial2.write(1);
  if (Serial2.available()) {
    
    int starter = (int)Serial2.read();
    
    if (starter==202) {
      Serial2.readBytes(armL, 8);
    }
    
  }
  
  Serial3.write(1);
  if (Serial3.available()) {
    
    int starter = (int)Serial3.read();
    
    if (starter==203) {
      Serial3.readBytes(legs, 8);
    }
    
  }
  
  
  if (logging) {                                         //logging the data to the SD card
    myFile = SD.open("dance1.txt", FILE_WRITE);
    now.toString(buf,len);
    //Serial.println(buf[0]);
    if (myFile) {
      //myFile.println(now.toString(buf,len));
      for (int i=12; i < 20; i++){
        myFile.print(buf[i]);
      }
      myFile.print("-");
      myFile.print("A:");
      for (int i = 0; i < 8; i++) {
        myFile.print((byte)armR[i]);
        myFile.print(",");
      }
      myFile.print("B:");
      for (int i = 0; i < 8; i++) {
        myFile.print((byte)armL[i]);
        myFile.print(",");
      }
      myFile.print("C:");
      for (int i = 0; i < 8; i++) {
        myFile.print((byte)legs[i]);
        myFile.print(",");
      }
      myFile.println("#");
      
      myFile.close();
    } else {
      //Serial.println("error opening file");       //Was there an SD error?
      logging = false;
      Serial.write(223);
      for (int i = 0; i < 8; i++) {
        Serial.write(1);
      }
    } 
  }
  
  
                                                          //Inout from Processing
  if (Serial.available()) {
    int recd = Serial.read(); 
    if (recd==49) {                                      //received a "1" ---> send position data!
      Serial.write(201);
      for (int i = 0; i < 8; i++) {
        Serial.write((byte)armR[i]);
      }
      
      Serial.write(202);
      for (int i = 0; i < 8; i++) {
        Serial.write((byte)armL[i]);
      }
      
      Serial.write(203);
      for (int i = 0; i < 8; i++) {
        Serial.write((byte)legs[i]);
      }
      
    } else if(recd==91) {                                 //received a "[" ---> reset first mini
        digitalWrite(A7, LOW);
        delay(1000);
        digitalWrite(A7, HIGH);
    } else if(recd==113) {                                //received a "q" ---> check battery level and report
        float batt = fuelGauge.getBatteryPercentage();
        //gaugeOutput();
        /*
        Serial.print((int) floor(batt));
        Serial.print(".");
        int frac = (batt - int(batt)) * 100;
        Serial.println(frac);
        //*/
        ///*
        Serial.write(220);
        Serial.write((byte) floor(batt));
        Serial.write(46);
        int frac = (batt - int(batt)) * 100;
        Serial.write((byte) frac);
        for (int i = 0; i < 5; i++) {
        Serial.write(1);
        }
        //*/
        
        if (batt<=3.00) {
         //Do emergency stuff here 
        }
    } else if(recd==32) {                                 //received a SPACEBAR ---> start/stop logging!
        logging = !logging;
        if (logging) {
          Serial.write(221);
          for (int i = 0; i < 8; i++) {
            Serial.write(1);
          }
        } else if (!logging) {
          Serial.write(222);
          for (int i = 0; i < 8; i++) {
            Serial.write(1);
          }
        }
    }
  }
  
  
  
  //delay(1000); 
}
void gaugeOutput() {
  Serial.print("Version: ");
  Serial.println(fuelGauge.getVersion());
  Serial.print("Alert Threshold: ");
  Serial.println(fuelGauge.getAlertThreshold());
  Serial.print("Alert Threshold Register Version: ");
  Serial.println(fuelGauge.getAlertThresholdRegister());
  Serial.print("Battery Voltage: ");
  Serial.println(fuelGauge.getBatteryVoltage());
  Serial.print("Battery Percentage: ");
  Serial.println(fuelGauge.getBatteryPercentage());
  Serial.print("Is Alerting? ");
  Serial.println(fuelGauge.isAlerting());
  Serial.print("Is Sleeping? ");
  Serial.println(fuelGauge.isSleeping());
  Serial.print("Is Sleeping Register Version? ");
  Serial.println(fuelGauge.isSleepingRegister()); 
  Serial.println("");
}