fjbart:
Can anyone direct me as to the best way to transfer data stored on an SD card via Embedded atmel ARM 7A3 to a PC via SD card reader?
Does the SD card need to be formatted with a FAT system? or is there a "driver that can read raw data from the card via the PC’s SD card reader?
under most *nix systems you can use a tool called “dd” which will dump the data from the card to a file. for example under linux you could do something like this:
#dd if=/dev/sda of=capture.dat
where sda is the sd/mmc card reader. i know there are similiar utilities for winblows but i don’t know their names.
implementing a filesystem is nice if you have the time and resources, but most of the time, it’s just as easy to just store the raw data.