Can you help me. We are working with msp430f2013 series on that am using SD16, but am facing one problem with that waht ever dig value am giving its not equal to or nearly equal to m input analog voltage. What may be the problem can help us?
IIRC, the specs of the SD16 on the '2013 indicate that if you are within 20% of the rails, the linearity suffers. In other words, you can use only the middle 60% of the voltage range between -Vref and +Vref.
Also, are you using the recommended capacitors on the reference supplies?
IIRC, the specs of the SD16 on the '2013 indicate that if you are within 20% of the rails, the linearity suffers. In other words, you can use only the middle 60% of the voltage range between -Vref and +Vref.
gm,
Wha tis IIRC? I was looking at the MSP430FE427 documentation and could not find anything similar.