Hello @ChenxinHu,
The ZED-F9P supports “Primary and Secondary Output” (from firmware version HPG 1.30). From the integration manual:
"
3.2.1 Introduction
u-blox GNSS receivers output various navigation results and data calculated as part of the
navigation solution. These include results such as position, altitude, velocity, status flags, accuracy
estimate figures, satellite/signal information and more.
The ZED-F9P can provide this output in two streams:
• Primary output: Reports the results of a full navigation solution using all capabilities of the
ZED-F9P, such as, for example, high precision positioning.
• Secondary output: Reports the results of a GNSS standalone navigation solution.
"
"
3.2.4 Example use cases
As an example, an application using a ZED-F9P can compare the secondary output solution to
be used as a sanity check against large errors in the RTK solution or errors originating from the
correction data.
"
So, if I understand correctly, logging both UBX-NAV-PVT and UBX-NAV2-PVT data would allow you to compare corrected and uncorrected data?
Please see the latest integration manual and interface description for more details:
https://www.u-blox.com/sites/default/fi … 010802.pdf
https://www.u-blox.com/sites/default/fi … 008968.pdf
Best wishes,
Paul