Hi everyone,
I’m encountering an issue while trying to upload a sketch to my SparkFun Thing Plus - ESP32-S3 board. Here’s the error message I’m receiving:
Sketch uses 301949 bytes (23%) of program storage space. Maximum is 1310720 bytes.
Global variables use 18660 bytes (5%) of dynamic memory, leaving 309020 bytes for local variables. Maximum is 327680 bytes.
esptool.py v4.6
Serial port COM38
Connecting…
A serial exception error occurred: Write timeout
Note: This error originates from pySerial. It is likely not a problem with esptool, but with the hardware connection or drivers.
For troubleshooting steps visit: Troubleshooting - ESP32 - — esptool.py latest documentation
I’ve reviewed SparkFun’s documentation for the board: Arduino Examples - SparkFun Thing Plus - ESP32-S3
Here’s what I’ve tried so far:
- esptool Version: Initially, I used
esptool v4.6(per the SparkFun docs). After receiving the error, I updated to the latestesptool v4.8.1, but the error persisted. - Board and Port Setup:
- Board: Selected “ESP32S3 Dev Module”
- USB Mode: Hardware CDC and JTAG
- USB CDC on Boot: Enabled
- Upload Mode: UART0 / Hardware CDC
- PSRAM: QSPI PSRAM
- Port: COM38 (verified in Device Manager)
All settings seem correct, and the COM port is the same as listed in Device Manager.
I’ve double-checked hardware connections, tried different cables, and reset the board multiple times, but no luck. If anyone has encountered this issue and found a fix, I’d appreciate your insights.
Thanks in advance!