Serial port

hi,

Can anyone tell me how to interface serial port with matlab or a driver code for serial port

Thanks

Regards

Sid

Presumably you just need something like a MAX3232 to interface the MSP320 to a PC COM port.

Leon

m using a laptop with no com 3 port…is der any solution to that…& is it possible by any code

THx

You need a USB-RS-232 converter, then. You need to write the code for the MSP430, of course.

Leon

As i am new to his MSP430 can you tell me where can i get a sample code for this or what will the code include…

Can anyone please tell me which code i can use from the code library for UART??

Which MSP430 are you using? Some need to use TimerA and some have hardware UART’s on them.

TI has sample code for both techniques.

Leon

M using MSP430Fg4618/2013 experimenter’s board

When i use USB to RS 232 converter, do i need to write some code for accessing USB or an UART code for kit & a matlab code would be fine?

USB to RS232 converters appear as COM ports under Windows. You can use them like normal serial ports.

i tried to use USB to RS232 but when i send data from USB the processor is not able to know that data is coming…wat is the solution to this. Can any one tell me which code can i use for serial port data transmit & receive

You can download the demo software from [here. There are two files - hal_uart.c and hal_uart.h. Include those into your project. That should get you started.

hth,

gm](http://www.ti.com/litv/zip/slac129a)