to answer my own question, for the benefit of others,…
well i’m running on raspios which is buster based,
sudo pip3 install sparkfun-qwiic
fails but you can run
sudo pip3 install sparkfun-qwiic-pca9685
sudo pip3 install sparkfun-pi-servo-hat
then a sample python program is below
import pi_servo_hat
import time
test = pi_servo_hat.PiServoHat()
#next line causes freqency to be set/reset to default 50hz but it can cause the servo’s to move.
test.restart()
motornum=0 #can be 0 to 15 for controlling each pwm motor attached
test.move_servo_position(motornum, 0) #start turning in one direction
time.sleep(1) #keep moving for 1sec
test.move_servo_position(motornum, 90) #start moving in the other direction
time.sleep(1) #keep mving for 1sec
test.move_servo_position(motornum 45) #stop moving
enjoy! 
in theory numbers between 0->45 move one way, 45-90 mve other way, 45 stationary.
each motor is not that accurate, so moves a different speed in one direction than the other, and moves in different speeds compared to each other. no doubt you could calibrate the rotation in each direction for each motor in order to be able to balance them.