SF Acconneer Radar XM125 A121 can't connect (error 'recv timeout') :(

Help! I connected this on windows with USB, installed acconeer explorer, installed the USB device drivers multiple times, flashed the acconeer firmware to the sensor successfully. I manually set baud rate to 115200 and also tried auto. Swopped multiple USB cables just in case. Tried everything. Nothing working. It sees the sensor board on com4 or whichever, but it cannot connect. The same error for two days now: ‘Failed to connect: recv timeout’.

So I gave up on the sparkfun integrated USB connection, and connected it via a usb-to-uart breakout board which I know works with another sensor. Again it can see the connection on com3 etc. Again it was able to flash the firmware to the A121 sensor. Again it cannot actually connect. Same error: ‘Failed to connect: recv timeout’.

I’ve read the other forum topics on this same error. None of them have any solutions that work for me. What’s going on?

Do you have a different pc/laptop you can test with it?