I’m struggling to figure out why my Pro RF is drawing so much current. I’d like to use it in a battery-powered application, but I’d need to cut the current draw dramatically.
I put the chip on a USB power monitor (with 10 mA resolution) while connected to TTN, and it was drawing a whopping 130 mA. Not sure if the radio is truly put to sleep, I did a test with a variety of boards, blink, and LowPower:
SF SAMD21 Dev:
-
blinking: <10 mA
-
sleeping: presumably <<10 mA
Adafruit Feather M0 + LoRa:
-
blinking: <10 mA
-
sleeping: presumably <<10 mA
-
running lmic (LoRa) example: < 10 mA (with the occasional spike for the radio)
SF Pro RF:
-
blinking: 60 mA !!!
-
sleeping: 10 mA !!!
-
running lmic library: 70 mA !!!
I’ve looked over the schematics and other than the LEDs, which should draw a handful of mA at most**, I don’t see what could be drawing the current.
Anyone have any idea why this is and what I can do about it? This is a cute, little board, but useless for any practical, battery-powered application in its current state.
Thanks.
**Not sure why SF puts a status LED on a battery-enabled board – seems a tad silly – but I can remove the physical draws, if needed.