The descriptions state that the I2C addresses are both x70.
I am having weird readings when I run the sensor through the mux… To confirm, do I need to change the I2C address on the mux to get it working?
Also related:
The description for the same sparkx version of the humidy/temp sensor states that the address is 0x71… but the datasheet states that the address is hardware defined and is 0x70… is this a typo??
I still wonder if the 0x71 address noted in the sparkx version is a typo? And should be 0x70? That is confusing me…
I’m using some sparkx versions and am wondering about this. I specifically bought sparkx version to avoid some of these issues so I’m just wondering if I’m doing something wrong or is it an actual typo?