Hi, I have been trying to debug an issue with not being able to use MCP23017 when hooked up through a pair of SparkFun PCA9615 boards. I soldered headers to connect to Raspberry Pi Zero, I am using about 15ft cat5 cable. Both boards have bounded VDDa and VDDb. I checked everything with a volt meter. I had some trouble seeing voltage on the far end at first, but I sorted it out.
Still I can’t see the device on the MCP23017 bus. I also hooked up an oscilloscope on the far end (PCA9615) and on the near end (Pi 0). What I noticed is a difference in the data line, specifically the low on the far end is not getting as low as on the near end. Please take a look at the attached screenshots. The wave is from the “detect devices” command
This is my closest lead as to why I can’t see the MCP23017.
I would really appreciate some help getting this to work.