Simon Game

Stupid question time!

Does the Simon game come pre-flashed with the firmware? I built my kit tonight and when I fired it up, I get nothing. Everything looks like it’s ok and I’m not new to SMT soldering, so I think I have a unprogrammed ATmega8.

I have an AVR programmer with a 10 pole target cable, but for the life of me, I cannot get anything to program. I am using a fresh install of WinAVR and the avrdude GUI. I THINK I set up avrdude correctly by showing it where avrdude.exe and avrdude.conf are. My programmer is an STKxxx variant.

Any help would be nice.

Thanks!

Jason -

Was wondering if you were able to get any further programming the kit. I finished the kit a few weeks ago (board dated 6-25-08). It’s my first experience soldering smd components but as far as I can tell everything is connected properly. I voltage tested the board to make sure that I am getting 5V out of it and have continuity tested every connection possible. I have been unable to program it either. I’ve tried two different cables to program - the usbtinyisp and using a parallel cable. Thought you might be able to provide some insight.

Thanks! :?

I’ve successfully programmed the Simon game with avrdude and my USBtinyISP programmer. I got the board at Make Faire, and it has the date 6-25-08. I soldered a 2x3 header to the ISP port on the board, and I’m using the 6-pin cable on the USBtinyISP.

Note that the Simon-v21 firmware, and the schematics at the Sparkfun page for Simon, do NOT match the board. The buttons and LEDs are on different ports/pins that what is shown in the schematic/firmware. I modified the firmware (by reading the traces on the board), rebuilt it with AVR Studio, and programmed it OK.