Mavam
1
I saw a program for a Heater controller, but did not understand how the pins got given a category, i.e. OUTPUT or INPUT.
Then I decide the pinMode were not given numbers because any pin can be picked to be what you want, (almost).
So, I modified the code to what I think it should look like.
Two questions;
Are my pinMode and digitalWrite done properly? See different font.
Can I leave documenting inside the code? Such as up_key, down_key, relay, etc. As in digitalWrite(2,down_key, high)
The down_key would be to document what the function is>>> Is that permissible?
Thanks, Mavam
Mavam
2
Arrgh, yes, pins 9 and 10 should say INPUT.
Mavam
3
Lesson Number 4 answered all my questions. 
Mavam
Deeat
4
Youtube and github always will help you)
The Arduino Language Reference at https://www.arduino.cc/reference/en/ can be very helpful as well.
https://www.arduino.cc/reference/en/lan … o/pinmode/
https://docs.arduino.cc/learn/microcont … gital-pins
You can either set your pinMode to INPUT_PULLUP, or set it to INPUT then digitalWrite that pin HIGH to enable the pullup.
PinMode (pin, mode), configuring pin mode
Pin: the number of the pin
Mode: The mode of the pin, Input: Input mode, OUTPUT: Output mode, Input_ PULLUP: Input pull-up mode
DigitalWrite (pin, value), specifying the pin output value
Pin: pin number
Value: Pin output value, HIGH: Output high level, LOW: Output low level.
DigitalRead (pin), reads the value of the pin, and calls this function to return the value of the pin, HIGH or LOW
Pin: pin number