Hi,
I have this code from UIPEthernet library:
/*
* UIPEthernet EchoServer example.
*
* UIPEthernet is a TCP/IP stack that can be used with a enc28j60 based
* Ethernet-shield.
*
* UIPEthernet uses the fine uIP stack by Adam Dunkels <adam@sics.se>
*
* -----------------
*
* This Hello World example sets up a server at 192.168.1.6 on port 1000.
* Telnet here to access the service. The uIP stack will also respond to
* pings to test if you have successfully established a TCP connection to
* the Arduino.
*
* This example was based upon uIP hello-world by Adam Dunkels <adam@sics.se>
* Ported to the Arduino IDE by Adam Nielsen <malvineous@shikadi.net>
* Adaption to Enc28J60 by Norbert Truchsess <norbert.truchsess@t-online.de>
*/
#include <UIPEthernet.h>
// The connection_data struct needs to be defined in an external file.
#include <UIPServer.h>
#include <UIPClient.h>
EthernetServer server = EthernetServer(1000);
void setup()
{
Serial.begin(9600);
uint8_t mac[6] = {0x00,0x01,0x02,0x03,0x04,0x05};
IPAddress myIP(192,168,0,6);
Ethernet.begin(mac,myIP);
server.begin();
}
void loop()
{
size_t size;
if (EthernetClient client = server.available())
{
if (client)
{
while((size = client.available()) > 0)
{
uint8_t* msg = (uint8_t*)malloc(size);
size = client.read(msg,size);
Serial.write(msg,size);
client.write(msg,size);
free(msg);
}
}
}
}
How can I use Serial.println() there to get something like:
Serial.println((String)msg);
please? I don’t know how to convert this uint8_t* msg to a char variable ![]()