Slodering/Desoldering pins of parts on a ground plane

How can I de-solder a pan/pin on a SMT/TH part when it is part of a ground plane? I’ve tried to use just my iron cranked up to a high temp, but it just doesn’t work.

I’m thinking I need to pre-heat the ground plane somehow (hot air pre-heater) so my iron can reflow the solder on the pad/pin better. I found these [preheaters, but they are expensive. Anyone got a home brew solution?](PCB Pre-heaters. Affordable Preheat for SMT, SMD, BGA. Lead-Free Solder. Compact Rework Preheat)

Ideally, you would build the board with thermals to avoid this problem.

The other option is to reflow the entire board using a skillet or toaster oven.

this probably isn’t what you want to hear but I have no problem using a hot-air smd rework station. works a trick.

Sometimes it helps to use a larger tip in your soldering iron - better and more contact improves heat transfer.

I think you just need a higher wattage iron.

My Metcal system doesn’t have any problems doing that sort of thing.

Leon

You all saying you can do this with hot air are either completely overheating your PCBs, have thermals, or are working on small PCBs. Removing a through hole component connected to a large ground plane requires a lot of heat. A pre-heater is the proper method if you’re using hot air.

If you want to do it with an iron - chipquik works remarkably well.

I never said I could do TH. Notice the part about “smd rework”. To be clear you are right about TH parts and hot air.

What does a thermal on a ground plane look like and how does it help in this situation? I can’t seem to get google to return any useful info for me on this.

Thanks.

It’s just a pad with spokes (four, usually) connecting it to the power plane. Most PCB packages can create them, as an option.

Leon

With a 45watt iron I haven’t had that much problem with thru-holes on ground planes up to TO-220 packages as long my solder braid is clean and I have a decent dab of flux.

Unfortunately the control board on my iron died last week, so I order an Aoyue 968. Hopefully it will be here soon.

leon_heller:
My Metcal system doesn’t have any problems doing that sort of thing.

Leon

I'd second that - Metcal is the King of irons and laughs in the face of groundplanes.