Can anyone tell me if the ROB-10551 is capable of 1/2, 1/4, 1/8 steps with the EasyDriver (ROB-12779)? I have been tinkering for a clock like application, but am only ever able to get 200 steps per full rotation with it. It doesn’t matter what values I assign to MS1 and MS2. I don’t see any documentation that implies it could do fractional steps, but I thought I would ask.
If not, is there a SFF motor like this one that can do fractional steps? I love the size and shape for my application, but would love better resolution than 1.8 degrees per step if possible.
*** EDIT ***
I figured it out. It’s 7.5 per step which can be divided down by 2, 4, and 8 it seems. I just didn’t read the datasheet close enough and assumed it was 200 steps to begin with. My math wasn’t so good.