SparkFun 20x4 SerLCD - RGB Backlight

Can anyone answer this question about th20 character by 4 line LCD display.

Are the characters in the display BLACK and the background of the display RGB values

  • or -

Are the characters of the display RGB values and the background BLACK (or dark)

From the video on the page with these types of displays it appears that at least one of the 16X2 LCD displays have characters with RGB values and a BLACK or dark background. This is the type of display I’m looking for but in the 20X4 display form factor.

The 20x4 LCD part number LCD-16398 and the 16x2 LCD part number LCD-16396 both have black characters that are on a RGB background.

LCD-16397 is a 16x2 display that has RGB characters on a black background.

Hope this helps, and have a great weekend!