SparkFun Edge failing on "make bootload"

Hi All

Followed all the steps in Windows 10 machine : facing the follwoing error: Please help me in resolving it.

$ make bootload

Compiling gcc …/src/main.c

Compiling gcc …/…/…/…/…/devices/am_devices_led.c

Compiling gcc …/…/…/…/…/utils/am_util_delay.c

Compiling gcc …/…/…/…/…/utils/am_util_faultisr.c

Compiling gcc …/…/…/…/…/utils/am_util_stdio.c

Compiling gcc startup_gcc.c

Compiling gcc …/src/tf_adc/tf_adc.c

…/src/tf_adc/tf_adc.c: In function ‘am_adc_isr’:

…/src/tf_adc/tf_adc.c:62:58: warning: passing argument 2 of ‘am_hal_adc_samples_read’ makes pointer from integer without a cast [-Wint-conversion]

62 | true,

| ^~~~

| |

| int

In file included from …/…/…/…/…/mcu/apollo3/am_mcu_apollo.h:132,

from …/src/tf_adc/tf_adc.c:1:

…/…/…/…/…/mcu/apollo3/hal/am_hal_adc.h:618:53: note: expected ‘uint32_t *’ {aka ‘long unsigned int *’} but argument is of type ‘int’

618 | uint32_t *pui32InSampleBuffer,

| ^~~~~~~~~

…/src/tf_adc/tf_adc.c:64:58: warning: passing argument 4 of ‘am_hal_adc_samples_read’ from incompatible pointer type [-Wincompatible-pointer-types]

64 | &ui32NumSamples,

| ^~~~~~~~~~~~~~~

| |

| uint32_t * {aka long unsigned int *}

In file included from …/…/…/…/…/mcu/apollo3/am_mcu_apollo.h:132,

from …/src/tf_adc/tf_adc.c:1:

…/…/…/…/…/mcu/apollo3/hal/am_hal_adc.h:620:64: note: expected ‘am_hal_adc_sample_t *’ {aka ‘struct *’} but argument is of type ‘uint32_t *’ {aka ‘long unsigned int *’}

620 | am_hal_adc_sample_t *pui32OutBuffer);

| ~~~~~~~~~^~

…/src/tf_adc/tf_adc.c:61:38: error: too many arguments to function ‘am_hal_adc_samples_read’

61 | if (AM_HAL_STATUS_SUCCESS != am_hal_adc_samples_read(g_ADCHandle,

| ^~~~~~~~~~~~~~~~~~~~~~~

In file included from …/…/…/…/…/mcu/apollo3/am_mcu_apollo.h:132,

from …/src/tf_adc/tf_adc.c:1:

…/…/…/…/…/mcu/apollo3/hal/am_hal_adc.h:617:19: note: declared here

617 | extern uint32_t am_hal_adc_samples_read(void *pHandle,

| ^~~~~~~~~~~~~~~~~~~~~~~

make: *** [Makefile:162: bin/tf_adc.o] Error 1

Thanks and Regard