Finally the sparkfun board edge boards arrived today ![]()
Following this well written guide : i am stuck with the following NoResponseError when trying to flash the code on the Ambiq, with the uart_wired_update.pyscript, that comes with tensorflow examples
opprud$ python3 tensorflow/lite/experimental/micro/tools/make/downloads/AmbiqSuite-Rel2.0.0/tools/apollo3_scripts/uart_wired_update.py -b 115200 /dev/cu.usbserial-1430 -r 1 -f main_nonsecure_wire.bin -i 6
MOJ/Connecting with Corvette over serial port /dev/cu.usbserial-1430…
Sending Hello.
No response for command 0x00000000
Traceback (most recent call last):
File “tensorflow/lite/experimental/micro/tools/make/downloads/AmbiqSuite-Rel2.0.0/tools/apollo3_scripts/uart_wired_update.py”, line 336, in
main()
File “tensorflow/lite/experimental/micro/tools/make/downloads/AmbiqSuite-Rel2.0.0/tools/apollo3_scripts/uart_wired_update.py”, line 38, in main
connect_device(ser)
File “tensorflow/lite/experimental/micro/tools/make/downloads/AmbiqSuite-Rel2.0.0/tools/apollo3_scripts/uart_wired_update.py”, line 58, in connect_device
response = send_command(hello, 88, ser)
File “tensorflow/lite/experimental/micro/tools/make/downloads/AmbiqSuite-Rel2.0.0/tools/apollo3_scripts/uart_wired_update.py”, line 235, in send_command
raise NoResponseError
main.NoResponseError
My setup:
Macbook pro, tried both old 15" & new 13"
Sparkfun serial basic breakout, USBC version (default jumped to 3v3)
FTDI 3v3 serial cable
I have tried
two different edge boards, with the correct Key14 & reset combo + misc variants and timing
legacy USB on old Macbook
new Macbook w USB C
FTDI 3v3 serial cable as alternative to sparkfun serial board
Running an alternative uart_boot_host.py script in tensorflow/lite/experimental/micro/tools/make/downloads/AmbiqSuite-Rel2.0.0/tools/bootloader_scripts/uart_boot_host.py, also no response
I can measure, with a scope, the handshake bytes ‘0x14’, ‘0x55’, ‘0x9d’, ‘0xe9’ ‘0x0’, ‘0x0’, ‘0x8’, ‘0x0’ being transmitted initially at 115200 on the TXO pin on the programming header - but the ambiq is not replying anything.
btw. The onboard demo is running, blue led flashing, an some “yes’s” are being recognized.
Any inputs welcome.