rev0:
Ok, I’ve tried many solutions and combinations after reading all the make issues in this forum, and still having no luck. The closest I’ve gotten is this, by holding down button 14 and running the command (letting the serial board do the reset with DTR):
You’ve gotten further then I have. I have seen lots of combinations of 14 reset undo reset start make etc. But nobody says when to let go of 14. Do you keep it pressed while doing the upload.
So far this board has been a TOTAL waste of time and money. Arduino had the right idea. Get something so people could play with the technology right away with examples. Sparkfun set the baud rate to the insane level of 921600 and so people have to recompile drivers just to talk to the board over a serial port.
I bought this board to work along the book tinyml. I think I’ve wasted my money.
The combindation of 14, reset on, reset off, make bootload, Sending hello, 14 off gives:
Connecting with Corvette over serial port /dev/ttyUSB0...
Sending Hello.
No response for command 0x00000000
received bytes 11
['0xd4', '0x70', '0x7', '0x87', '0x84', '0x80', '0x80', '0x83', '0x80', '0x80', '0x80']
Traceback (most recent call last):
File "../../../bsp/tools/uart_wired_update_sparkfun.py", line 343, in <module>
main()
File "../../../bsp/tools/uart_wired_update_sparkfun.py", line 44, in main
connect_device(ser)
File "../../../bsp/tools/uart_wired_update_sparkfun.py", line 63, in connect_device
response = send_command(hello, 88, ser)
File "../../../bsp/tools/uart_wired_update_sparkfun.py", line 240, in send_command
raise NoResponseError
__main__.NoResponseError
Makefile:197: recipe for target 'bootload' failed
make: *** [bootload] Error 1
The combination of
14 reset on reset off, 14 off makeboot gives
Sending Hello.
No response for command 0x00000000
Traceback (most recent call last):
File "../../../bsp/tools/uart_wired_update_sparkfun.py", line 343, in <module>
main()
File "../../../bsp/tools/uart_wired_update_sparkfun.py", line 44, in main
connect_device(ser)
File "../../../bsp/tools/uart_wired_update_sparkfun.py", line 63, in connect_device
response = send_command(hello, 88, ser)
File "../../../bsp/tools/uart_wired_update_sparkfun.py", line 240, in send_command
raise NoResponseError
__main__.NoResponseError
Makefile:197: recipe for target 'bootload' failed
make: *** [bootload] Error 1